FB#.IDENTIFIED

Description

This parameter is set according to FB#.SELECT on drive power up if FB#.SELECT is not –1; otherwise the parameter value is read from the drive memory.

Type

Description

0

Unknown
1 No encoder

10

Incremental encoder with A/B Quad, marker pulse and Hall

11

Incremental encoder with A/B Quad, marker pulse and no Hall

13 Step/Direction
14 Clockwise/Counter-clockwise

20

Sine Encoder , with marker pulse and Hall

21

Sine encoder , with marker pulse & No Halls

30

EnDat 2.1 with Sine Cosine

31

EnDat 2.2

34

BiSS"Bi-directional Serial Synchronous interface" An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder Mode C

40

Resolver

41

SFD (Smart Feedback DeviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position)

45 SFD3
46 Hiperface DSL
63 Simulated Motor

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

FB#.SELECT

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen